6/2/2006 6:48 AM | |
Posts: 42 Rating: (0) |
Hi, Thanks for the reply. I am trying to create the block in a CFC by compiling the CFC as a FB. How should i proceeed in this case? CSS6 |
6/5/2006 7:14 AM | |
Posts: 42 Rating: (0) |
Hi, Thanks for the reply. How do i define this Struct?Is it a block? I cant locate it in my libraries. |
2/7/2007 4:05 AM | |
Posts: 73 Rating: (20) |
Hello, You do not have to create the structures manually as there are many attributes which must be entered. Simply drag the parameterof the FB on the CFC chart to the first open NAME field in the Chart INPUT/OUTPUT Window. See attached picture I hope this helps. Regards AttachmentPresentation1.zip (811 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on