1/4/2012 10:07 AM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating: (17) |
Hey mothilal, is there any useful information in the diagnostic buffer? Best Regards Manfred |
1/20/2012 1:10 PM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating: (17) |
Hey Monthilal, The usable memory cards are described in the Simotion compatibility list.This file is located on the SCOUT DVD (SCOUT Addons/1_Important/compatibility) or here http://support.automation.siemens.com/WW/view/en/18857317 Look to chapter 2.4. Therefore you have to be Online with SIMOTION C. The correct procedure is described in the SCOUT Online help: Use Format MEMORY CARD and overall reset to format the memory card on which you save project data. The memory card must be formatted before it is used for the first time. During formatting, all data on the MEMORY CARD is deleted and a file system is created. An overall reset is performed on the memory card before formatting. Regards Manfred |
Follow us on