Industry Online Support
Technical Forum
1/24/2012 7:25 PM | |
Posts: 36 Rating: (0) |
Hello Everybody, I am having problem while opening the project in WinCC Flex 2 008 SP1.I am using Windows XP Pro with SP3. The error popup Shows "Cannot connect configured server, Make sure that MSSQLWinCC Express is running and not disabled. If the error persists, re-install the WinCC flex DB server". The attachment is here. So help me. Thanks and Regards. BMP. AttachmentError While opening Project in WinCC flex.pdf (515 Downloads) |
1/25/2012 7:34 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Check it there - sql license message when client try to connect to the server Best regards, Hristo Mihalev |
1/25/2012 7:49 AM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Hi, Also, read this /tf/WW/en/Posts/27883 |
Best regards, |
|
1/2/2013 8:16 PM | |
Posts: 5 Rating: (1) |
Hello man i have the same problem i've tried everything from checking to reinstalling and nothing works can someone plzase help me! |
1/7/2013 2:35 PM | |
Posts: 3037 Rating: (192)
|
Hello, You do the point 1.4 of the following link. http://support.automation.siemens.com/WW/view/en/29420408 Tweety |
Follow us on