Industry Online Support
Technical Forum
1/24/2012 1:54 PM | |
Posts: 37 Rating: (0) |
Hello Everyone I am using 5 nos of TDC CPU551 in single Rack. SFC's are put in 3rd CPU. There is no error while compilation and downloading of CFC & SFC in CPU. After opening one of the SFC and going in TEST mode it gives error which is attached . After clicking OK , it goes in RUN mode but I am unable to to START/STOP or do anything. All the transition blocks are connected to charts and all charts are available.I have attached Screenshot. Please help. I havealos includedscreenshots of SFCI block also showing error code :32 in QFA. AttachmentSFC Error.zip (109 Downloads) |
Last edited by: himanshu at: 1/25/2012 10:14 AMLast edited by: himanshu at: 1/24/2012 3:44 PM |
|
1/25/2012 10:10 AM | |
Joined: 8/25/2006 Last visit: 4/26/2024 Posts: 2203 Rating: (277)
|
Hello. Have you configured function block 'SFC' in CFC-chart for your SFC-chart? |
1/25/2012 10:16 AM | |
Posts: 37 Rating: (0) |
yes i have included SFCI block in my chart |
Follow us on