1/31/2012 12:52 AM | |
Posts: 2661 Rating: (279)
|
You do not need to add the new ES in the old multiproject (either project or PC station). Just open the old project from the new station over the network(File/Open/Multiprojects/Browse). Of course this is independent of the standalone “test project” you’ll create to commission the new PLC. See following app note: PCS 7 Multiproject / Multi-user Engineering |
Follow us on