Industry Online Support
Technical Forum
1/31/2012 10:00 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Greeting, I have reinstall the window & Step7 V5.5 with SP1 then install simotion, WinCC flex, & WinCC. Befor installation of simotion, and other software i cheked opertor control and monitoring was enabling successfully after installation of another software again problem appear simatic stop working and unexpectedly close. One project which have atteributes on DB's and AS/OS engineering is not opening when i switched from small icon to list the simtaic manager held and stop working regarding administrator rights i have attached please see in image. Thanks, Regarded, AttachmentPictures.zip (76 Downloads) |
MS |
|
1/31/2012 10:04 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Operation Control & Monitoring Best regards O_Moderator |
Follow us on