Industry Online Support
Technical Forum
2/2/2012 1:27 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello krishnakumar_eee, It's recommended by default to use the latest software which is STEP 7 v11 SP2. Try with TSEND_C and TRCV_C, which is the combination of TCON, TSEND and TDISCON likewise TCON, TRCV, TDISCON. You have to check where the Connect and Disconnect instruction is used and is it done in a sequential manner. If either of this is not happening, there is possibility that it will work once when there is a warm restart (which is noting but your power cycle) Or check this for tested application - Ethernet Communication: Data Exchange S7-1200 <-> S7-1200 (CE-X17) |
Like it? Rate it! |
|
2/3/2012 7:28 AM | |
Posts: 30 Rating: (2) |
Sir, With Regards, P.Krishnakumar
|
Follow us on