8/12/2011 4:46 PM | |
Joined: 5/7/2011 Last visit: 11/4/2023 Posts: 14 Rating: (2) |
I use Safari Browser on PC and MAC and i have same problem as you write. |
12/22/2011 10:07 PM | |
Posts: 19 Rating: (0) |
Tested with Nintendo Wii (Opera browser). it is NOT necessary the certificate. it Works!! |
1/31/2012 2:10 PM | |
Posts: 20 Rating: (1) |
Is there a solution found or fix-update for the problems with Google Chrome and Safari with the S7-1200 webserver? |
2/1/2012 11:44 AM | |
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Hello, You can try use the add-on "IE TAB" for Chrome.https://chrome.google.com/webstore/detail/hehijbfgiekmjfkfjpbkbammjbdenadd I didn't test it yet with 1200 web server, but I think it will work. I Know that is not the same, but it's is an option for now. Regards
|
Gabriel de Oliveira |
|
2/3/2012 10:30 AM | |
Posts: 20 Rating: (1) |
I found out that Google Chrome, Safari and Android are all using "Webkit Open Source" as framework on the core off the application (Chrome&Safari) or as total browser itself (Android). There is a possibility that here lies the problem. Still looking for a solution.. if anyone has an idea, everything is welcome ;) Webkit Open Source: http://www.webkit.org/ http://trac.webkit.org/wiki |
Last edited by: Ivo vd E. at: 2/3/2012 10:33 AMadded websites |
|
Follow us on