Industry Online Support
Technical Forum
2/3/2012 10:17 AM | |
Posts: 3 Rating: (0) |
Hi all Hi have a problem with a TCP/IP connection between WCC and a S7 315 2PN DP. First, I can not import an IE General from a XDBon the station configuration... An error message say "This component is not installed" On the configurator console, the ethernet card is on error "no ip adress etc.." But I have installed the last driver, reboot the PC etc... Can you help me? See the image AttachmentTCP Problem.pdf (73 Downloads) |
2/3/2012 3:41 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi It seems that your LAN driver is not OK. Try Reinstalling the same. and check that same. Have fun... |
Jazz |
|
Follow us on