2/17/2012 3:38 PM | |
Posts: 6 Rating: (0) |
Toeternietoe your ladder is simple but it doesn't loop. I need it to loop until the hopper sensor is satisfied.
|
Last edited by: biffidum at: 2/17/2012 3:44 PM |
|
2/17/2012 3:43 PM | |
Posts: 6 Rating: (0) |
cdrshortyours almost does it, but your ladder requires 2 pulses from the pressure sensor to switch cylinder directions. This will not be possible as the cylinder will stop advancing on the first pulse and as a result not deliver pressure for a second pulse. Someone also mentioned that an 0BA0 can't invert a sensor input - that is incorrect. Under group functions you will see it has the NOT function which will serve to invert the input. True the 0BA0 does not have the option of directly inverting any input by simply highlighting the small block at the junction.
|
Last edited by: biffidum at: 2/17/2012 3:45 PM |
|
2/17/2012 7:36 PM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
@Marcjan Attachmentvalve change 0ba0.zip (286 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
Follow us on