2/13/2012 3:25 PM | |
Joined: 8/31/2010 Last visit: 5/10/2024 Posts: 1509 Rating: (222) |
Check this for your requirement - * SIMATIC STEP 7 Basic V10.5 Getting Started Manual/ GettingStarted Project- Download Page * Controlled positioning with S7-1200 via pulse/direction interface (CE-X7) * Which Motion Control functions are there in STEP 7 (TIA Portal) V11 and how do you use these functions? |
Like it? Rate it! |
|
2/15/2012 7:23 AM | |
Posts: 8 Rating: (0) |
Hello, Sorry but I can't upload program because pup up error, i attached screen this program. I tested this program and he work properly. How he work? When the I0.4(start) change from 0 to 1 then axis is active, then MC_Home is execute. If the point switch(your sensor) is detected the motor are reduced the speed and change the direction, if the point switch is detected one more time, the motor change direction again, and finally if the point switch is detected third time, he should be stopped. This apparent from picture in homing configuration. Good luck Przemos169 AttachmentProgram_screen.zip (800 Downloads) |
Follow us on