Industry Online Support
Technical Forum
2/16/2012 11:57 AM | |
Posts: 3037 Rating: (192)
|
Hello, Can you post a screenshot of your Error message? Which panel do you use? Do you have problems with panel and plc? Tweety |
2/16/2012 3:35 PM | |
Posts: 23 Rating: (0) |
Apart from being unable to auto-detect hardware the PLC seems to working fine. I am able to implement basic programs. I have attached a screeshot of the error message I am getting. Thanks in advance.
AttachmentScreenshot Error.pdf (491 Downloads) |
2/17/2012 11:37 AM | |
Posts: 3037 Rating: (192)
|
Hello, Do you check all things in the error message box "Cannot perform transfer"? You can find more information about download via ethernet to a panel in the following FAQ. Wie kann eine WinCC (TIA Portal) Projektierung über Ethernet auf ein Bediengerät übertragen werden? This FAQ is translated to englishat the moment. Tweety |
2/17/2012 12:36 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello Tweety, Hope this english version is in preparation. |
Like it? Rate it! |
|
2/22/2012 2:40 PM | |
Posts: 23 Rating: (0) |
By the way I dont' have an actual HMI device attached. I'm trying to set up the HMI design part of the Step 7 software. |
Follow us on