2/29/2012 10:18 AM | |||||||||||||||||||||||||
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello worldleader, That is a problemin theSIMATICSelectiontool. Don't get annoyed. The DP Master module can be connected with the IM151-8 CPU. You can checkthe samein either Catalogs or Brochures or Manual (Operating Instruction of ET200S: CPU/IM 151-8 PN/DP) or any of the below - Function of the IM 151-8 PN/DP CPU interface module - Properties of the IM 151-8 PN/DP CPU interface module - Properties of the DP master module Finally a configuration example for you with PROFIBUS DP Master module with CPU 151-8 PN/DP
Example configurations
Let's communicate this to Siemens. Request the moderators to take it up to the right team. |
||||||||||||||||||||||||
Last edited by: Ganes10 at: 2/29/2012 10:22 AMmessage to moderator Like it? Rate it! |
|||||||||||||||||||||||||
3/2/2012 6:51 AM | |
Posts: 22 Rating: (1) |
It's very kind of you! |
Follow us on