Industry Online Support
Technical Forum
3/1/2012 7:53 AM | |
Posts: 8 Rating: (0) |
Hello Everyone. I am using safety PLC ET200PRO: IM 154-8F PN/DP CPU, 512KB and interface module, IM 154-4 PN HIGHFEATURE FOR CONNECTION TO PROFINET. when i am configuring hardware with Im154 and Fswitch 6ES7148-4FS00-0AB0, after save and compile, there were "system inconsistency" error pls help. i already installed f configuration pack F-Config_V55SP2 and FConfig_V55SP9 Error occurs:- 1. The hardware in a PROFINET IO or mixed environment (PROFINET IO and PROFIBUS DP) has to support the bus profile PROFIsafe in V2-MODE. 2. The "Replace device without exchangeable medium" function cannot be used for IO device "SIMATIC 300(1)\(1) IM154-4PN". Best Regards, Chetansing Patil Attachmentsimatic 300(1).zip (230 Downloads) |
Last edited by: CMP at: 3/1/2012 8:17 AMLast edited by: CMP at: 3/1/2012 8:06 AMConfiguration attached. |
|
Follow us on