Industry Online Support
Technical Forum
3/9/2012 1:36 PM | |
Joined: 5/26/2007 Last visit: 9/3/2024 Posts: 127 Rating: (3) |
i got a 6es73141ae020ab0 with a MC (flash eprom 16kB) a cp342-2, a 3211bl00 and a 3221bl00 install. is there a posibility to have a different program in MC and in CPU? when i upload from cpu, in h/w config it show that my di and do as standard module. then i switch off the cpu and turn the key to stop mode, and switch on again. this time i got a different program. i.e: in my first upload i have fc1, then in my second upload i donot have it but i got fc8. some of the fc is same but with different size, when i look inside the fc code, i found the code is almost the same but with the second upload there are some missing line in several network. AttachmentCPU.zip (112 Downloads) |
3/9/2012 2:42 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Well do a memeory reset and then download entire program & Hardware and check. Have fun... |
Jazz |
|
3/10/2012 5:03 AM | |
Posts: 1064 Rating: (72) |
What version of step 7 are you using and do you have the current hardware catalog installed ? |
3/10/2012 7:19 AM | |
Joined: 5/26/2007 Last visit: 9/3/2024 Posts: 127 Rating: (3) |
step 7 v5.4 yes i have the latest h/w catalog. |
Follow us on