8/17/2011 7:39 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (43) |
Hello all, Short question. My 313C CPU has 3 integrated pulse counters. As I understand, most of the 16 first Di and 3Do will be used by the pulse counter. See page 192 of this document: Here! My question, if I only use 1 pulse counter (channel 0), do I still need to reserve all the inputs and outputs? Ton |
8/18/2011 9:28 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
If only one counterchannel isused the other onboard i/o can be used digital, see attached part of the manual. All other channels must be set to not configured. Regards, Marcjan Attachmentforum313c.pdf (429 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
8/18/2011 9:48 AM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (43) |
Great! Thank you! |
4/2/2012 7:13 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (43) |
Please find attached the screenshots. I don't think the problem is there tho. I think its because of the speed of the pulses + the length of the cable... But I am not sure.. Thanks!
Attachmentcounter.pdf (284 Downloads) |
Follow us on