3/13/2012 6:52 AM | |
Posts: 165 Rating: (25) |
hello experts Is it possible to get a "rated torque @ zero speed" in Induction motor ? Thanks Regards Mothilal |
3/14/2012 5:18 AM | |
Posts: 165 Rating: (25) |
Hi PISCEAN Thanks for your reply. Hmmm .. What about servo motor? can we get the servo motor rated torque at any desired speed ? Regards Mothilal |
3/14/2012 6:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hi Mothilal, Servo motor generally two torque ratings are mentioned One at zero speed i.e. static torque (Mo)& the other available during entier speed range of motor upto its rated speed. (Mn) Depending upon motor type number & comparing its speed torque motor user can be able to read torque available at particular speed. Please find attached here with sheet of speed torque graph of Siemens make servo motor, which you can refer. Hope this help you. DEEP. AttachmentSpeed Torque graph.pdf (916 Downloads) |
This contribution was helpful to1 thankful Users |
4/18/2012 8:41 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
With AC drives, I think its possible Have a look at attachment This will also helpful for yout another Query Regards, Devesh Vithani AttachmentAC Motors.pdf (863 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
Follow us on