4/19/2012 9:58 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Check itCompare between PLC S7-1200 and PLC S7-200This was a long discussion on that time. With known in advance result. best regards, Hristo Mihalev
|
4/20/2012 12:04 PM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046) |
Hello Gorp as they say"one man's trash (aka crap) is another man's treasure", and I for one appreciate Anchobi's point of view and also believe it is actually on topic. Could it bethat your (very off topic by the way) reply is simply an indication that you ran out of technical arguments? Anyhow, no harm done (I think), thisis a Forum after all and everyone is entilted to their point of view, so here is mine: @ Vispute Prashant: Yes, there are "limitations" with the 1200 when you compare it to a 300 or 400, itis however a "Micro" PLC(also pricewise). Considering that it offers features such as ProfiNet I/O Controller, DP Master, DP Slave, LongREAL etc., it does actually pack quitea punch in my humble opinion (more so ifand when it will support I-Device and Safety Integrated). Sure STL is sadly missing and I had my rant about thissome time ago in a different thread. I am still hopeful it will supported on day though (truth be told, it doesalready support STL,Siemens simply decided to lock STL out of the TIAP Portal Step 7when you use a 1200). |
Last edited by: fritz at: 4/20/2012 12:06 PMtypos Cheers |
|
Follow us on