4/24/2012 9:30 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Hello SolutionFinder, here is the link to the manual: http://www.google.de/url?sa=t&rct=j&q=s5%20cpu%20928%20operating%20instructions&source=web&cd=2&ved=0CEMQFjAB&url=http%3A%2F%2Fcache.automation.siemens.com%2Fdnl%2FTc%2FTc5MTgyMzEA_1085940_HB%2Fpa928ben.pdf&ei=o1KWT4T9L4af0QWSoPW-Dg&usg=AFQjCNHwA4ciQviEmf4I6z4wTfAi8a6CIQ Look at the operation list / arithmetic operations. There you will find examples as well. Do you need to scale an analog input/output signal or do you want to generally scale a value? What are the requirements of your function block? Input parameters and format? Output parameters and format? i.e.: Input Value (real) Input min. (real) Input max. (real) .... .... Regards. |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
4/24/2012 9:35 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Dear SolutionFinder, |
Give us your feedback and show us your respect! |
|
This contribution was helpful to1 thankful Users |
4/24/2012 1:23 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating: (90) |
Hi solutionfinder, Here is an example on how to convert 4-20mA AI. Kind regards, BV AttachmentFB14@@ST.zip (138 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on