Industry Online Support
Technical Forum
4/29/2012 11:16 AM | |
Posts: 57 Rating: (0) |
Hi, Except PC mounting kit ,what are the other interfacing tools which can be used to communicate to a Sinamics G120 CU240S-DP control unit? |
4/29/2012 11:27 AM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324) |
Hi, as per the attached extract, you only have three possibilities, you already mentioned the PC Interface kit, you can also commission/communicate via the Profibus port - both of which can be used with the free downloadable Starter software. For repeat programming, you can use the SD card slot (ideal for OEM's producing hundreds of drives with the same configuration)
Regards, Graeme AttachmentCU240S DP.pdf (167 Downloads) |
Follow us on