5/1/2012 5:17 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, It happens often that the current firmware version is higher than the max. version found in HWconfig. In fact, anew FW version will mostly only appear in HWconfig if new parameters areavailable in that FW version compared the previous ones. You can trace also the different update entries provided in the support pages. In the V2.4 update entry, http://support.automation.siemens.com/WW/view/en/50583778 it iscleraly stated that V2.4 is configured as V2.2 In the V2.5http://support.automation.siemens.com/WW/view/en/57075905 and in V2.6 http://support.automation.siemens.com/WW/view/en/59038647 the entries state that there are no functional changes. In other words, V2.2 is fine for configuration |
Best regards |
|
Follow us on