3/30/2009 3:17 PM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, Have you the release of the CP5711? see: http://support.automation.siemens.com/WW/view/en/6GK1571-1AA00 |
Smurf |
|
4/14/2009 5:40 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
Please notechapter 3 of the "Released for Delivery" In my words:To use theCP5711 you need: SIMATIC NET V7.1 SP1 or STEP7 V5.4 SP5 And STEP7 V5.4 SP5 is actual not released! (status of 14. April 2009). I tested the CP5711 (in a virtual machine) withSTEP7 V5.4 SP4, SIMATIC NET V7.1 SP1 and WinCC Flex 2008 (I think with SP1), andit worked. |
|
|
4/5/2012 10:59 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Can we use thisadapter ?? It supports 32 bit.
|
4/22/2012 12:50 PM | |
Joined: 11/18/2009 Last visit: 6/4/2024 Posts: 262 Rating: (18) |
Hi Shanny I had same problem. I have bought this adapter and I use it with CP 5512. I have connected it to SIMATIC S7-400 and to SENTRON WL with COM15. http://www.delock.de/produkte/G_66214/merkmale.html It works fine. |
5/1/2012 5:43 PM | |
Posts: 947 Rating: (45) |
Hi, shanny Cp5512 discontinued. To replace them, use CP5711. For his work need only 5V, for example, from USB, unlike the adapter MPI-USB, which should be 24V and which is not all connectors MPI / Profibus. In addition, this CP, and it supports more features, including 12MBod p.s. did not notice the date of the first post. Now all the posts 2012year irrelevant, since the question was asked a few years earlier. With the "necro"post colleagues |
Last edited by: gre_m at: 5/1/2012 6:00 PM |
|
5/3/2012 8:22 AM | |
Joined: 11/18/2009 Last visit: 6/4/2024 Posts: 262 Rating: (18) |
Similar solutions can be found. I have given him same solution as you but with other adapter. |
Follow us on