5/7/2012 2:46 PM | |
Posts: 16 Rating: (0) |
Hi, |
5/7/2012 2:51 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Hi, Check attached. Should be clear for you. |
Best regards, |
|
5/7/2012 3:16 PM | |
Posts: 16 Rating: (0) |
|
This contribution was helpful to1 thankful Users |
5/7/2012 6:36 PM | |
Posts: 16 Rating: (0) |
It is possible to disable the active hightlight row ? Becuase if you only have one alarm the row will be show with the active highlight color... |
5/7/2012 6:58 PM | |
Posts: 16 Rating: (0) |
Are there a possible to check if there are any active alarms ? |
5/7/2012 8:33 PM | |
Posts: 559 Rating: (87) |
Dear Urban.matsson, Yes it is possible to set to view only active alarms also. You Please go to the properties of alarm window, there you will find UnAcknowledged & Pending Etc. So you select Unacknowled alarms only, That will display only active alarms. Please go through the below FAQ which will be more helpful to you. How do you display messages in WinCC flexible? |
Follow us on