5/17/2012 4:02 PM | |
Posts: 691 Rating: (36) |
Is it that you you are trying to download in MPI , but your CPU MPI Port is configured in DP? Can you send us the Pics of PLCSIM and CPU Configured? |
5/17/2012 4:37 PM | |
Posts: 559 Rating: (87) |
Dear sureking, When you are starting PLCSim, Please check that PG/PC interface didn't automatically change to the appropriate one (PLCSIM MPI in Your case). If yes then change it manually and also try with different project and MPI, and after this it should started to work normally. Also refer to below Post which has same problem as you /tf/WW/en/Posts/73323 Best.. |
5/17/2012 4:58 PM | |
Posts: 14 Rating: (0) |
I have already done that. I had checked that link before I posted my question. |
Follow us on