Industry Online Support
Technical Forum
5/23/2012 10:55 AM | |
Posts: 18 Rating: (0) |
....Thank you so much for your understanding and helping, I solved that problem in file.The Motors(1,2,3) run respectively. What I mean that is M1 runs for 5s.After M1 is off,M2 runs for 5s.After M2 is off,M3 runs for 5s..And this system will be go on Until I press the stop button.... So I solved What I say above problem..Actually my aim is to add some contact just like I0.1,I0.2,I0.3.The summary of the purpose of the program is following Firstly,The motors will be run as above,respectively but, What I want to do? 1)when I press the I0.1,the m1 will be off and the other motors that motor2 and motor3 will be run respectively(5s M2, 5s M3 and continue like this until when I press the stop button)..And The system will be run as before If I give up pressing to I0.1 button 2) When I press the I0.2 the M2 will be off....and same process(m1 and m3 will be run respectively and always) 3)When I press the I0.3 the M3 will be off....and same process(m1 and m2 will be run respectively and always) Attachment3MotorsRUN_respectively.zip (238 Downloads) |
5/23/2012 11:39 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread the program helping s7-1200 TIA portal. Best regards O_Moderator |
Follow us on