6/10/2011 10:41 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Smith Predictor for Control of Processes with Dead Times Some processes respond with high dead time.Dead time is one of the natural properties of a process.Consider the temperature of liquid in a tank should be regulated by steam(control valve on steam).When you open the control valve (Step change to process) more steam flows into the exchanger, conduction and convection are necessary to increase the value read by temperature transmitter.
Here is a configuration and also a simulation with different parameters: http://csd.newcastle.edu.au/simulations/roll_sim2.html From 07/2009 the function provided in advanced process control of PCS 7 V7.1. Following topics covered here: 1-Basic Principles of the Smith-Predictor 2-Implementation of the Smith-Predictor 3-Identification of the Process Model from Learning Data 4-Parameterization and Commissioning 5-Simulation Example 6-The Smith-Predictor in the Operation Phase Hope to helps hdhosseini |
This contribution was helpful to1 thankful Users |
6/11/2011 2:26 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Yes I know the point.When we think of a control loop, the idea is an ideal set of subsystem interconnected together and make a whole.Instrument and mechanical deficiency paralyze the loop. The goal and the ideal of a control engineer is to design the loop in ideal form and consider some constrains (limiting points).In real world, operators and maintenance team are available to take care of the system and rectify the deficiencies. Every function or product we are using, have deep theorical background which is hidden from the user.I recommend reading section 1-1 of the following book, when the author describes the terms such as quality of control and process optimization and ... . but what about control performance?
regards |
Last edited by: hdhosseini at: 6/11/2011 2:29 AM |
|
This contribution was helpful to2 thankful Users |
Follow us on