5/7/2012 6:38 PM | |
Posts: 133 Rating: (9) |
Hi this is a tough one. The default screen configurations in the OS project editor is four screens. There might be a solution if you set the resolution of your overview page so that itoverlaps two screens. However this is not recomended. I have seen it being done on a project. Attachmentscreen config.pdf (201 Downloads) |
5/8/2012 11:02 AM | |
Joined: 10/9/2007 Last visit: 4/22/2024 Posts: 1239 Rating: (115) |
Hi Ensar We are on the definition phase. I just know that must have 46". There are some companies like this http://www.multi-monitors.com/which could also offer a solution. But I wouldn't do this on a substation. For the simplicity and to avoid headaches with drivers, compatibility, resolution and so on, I'll go with 2 clients. Mike |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on