5/8/2012 4:21 PM | |
Joined: 3/8/2011 Last visit: 9/3/2024 Posts: 49 Rating: (4)
|
Hello, to get the respective drivers please contact your technical support center or send him a service request: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&dws=csmysupportsrna&objId=38718979&framey=560&iframeurl=support%2FSR%2FIndex%2Easpx%3Fnonav%3Dtrue%26pageNr%3D0%26lang%3Den&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus Have a nice day |
5/8/2012 5:05 PM | |
Posts: 34 Rating: (0) |
My suggestion is>> Don't attempt such experiment for your betterment. |
7/4/2012 4:43 PM | |||||||||||||||||||||
Joined: 7/3/2012 Last visit: 3/26/2024 Posts: 18 Rating: (2) |
Hello cbcx, i hope this is the answer you waited for: 1., 2., 3., In general Win7 64-Bit is released for sales since April,in deliverysinceMay 8th and is one ofthree OS options for the Field PG M3: Operating system options and work memory:
*) The operating system option "C" is subject to a surcharge! If your Field PG M3 originally hadWin7 32-Bit installed, the licence allows you to install Win7 64-Bit legally. This can be done using a current Field PG M3 image, including all required drivers. Siemens personal should be able to support here(details: http://support.automation.siemens.com/WW/view/en/60466787) 4. STEP 7 Safety Advanced V11 with 64-bit support is released since February: http://support.automation.siemens.com/WW/view/en/58205193 Regards, Toni4711 |
||||||||||||||||||||
This contribution was helpful to2 thankful Users |
Follow us on