5/19/2012 1:11 PM | |
Posts: 1064 Rating: (72) |
depend sif you want or need to use the s7-1200 seriesprocessors for them you need tia |
This contribution was helpful to1 thankful Users |
5/19/2012 1:15 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (42) |
Hi! No we only use 300 series. |
5/19/2012 8:19 PM | |
Joined: 11/18/2009 Last visit: 8/17/2023 Posts: 262 Rating: (18) |
Step7 is simply great especially for 300 and 400. |
This contribution was helpful to1 thankful Users |
5/19/2012 8:29 PM | |
Posts: 1064 Rating: (72) |
if you don't need the functions of tia then stick to step 7 at least until you hav eto change |
This contribution was helpful to1 thankful Users |
5/19/2012 9:33 PM | |
Joined: 4/20/2007 Last visit: 2/6/2024 Posts: 724 Rating: (42) |
well, I got both with my latest update.. |
7/6/2012 10:22 AM | |
Posts: 7 Rating: (0) |
Hi if you need redondant scada server you can't use TIA. On my actual project i have to program PLC via TIA (S7-1200) and develop HMI with WinCC v7 |
Follow us on