Industry Online Support
Technical Forum
7/10/2012 7:05 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Before starting otimisation, have you adjust the rated unit currents? Please check the attached sheet. Attachment6RA80 commissioning.pdf (405 Downloads) |
7/14/2012 5:39 AM | |
Posts: 22 Rating: (0) |
hello... everything was setted well... afetr auto optimisation I did the manual optimsation of current controller and step responces OK howevevr again I tried to do auto optimisation then actual current goes upto 220%. Generally it must go up 70% and some peaks (spikes) can go up to 120% as my experince in 6RA70. Kindly do the needful. Thnks & regards, DK |
Follow us on