1/18/2012 8:38 AM | |
Posts: 19 Rating: (0) |
Dears, I'm using CPU315-2PN/DP - 2EH14 - 0AB0 and in SIMANTIC Manager I configured like as in the attachment. but I can not download to CPU. Do I need insert the a MMC (Memory Micro Card) because I dont insert it yet? And in the Configuration HW, do we need to insert CP343-1 (Communication Port)? On this CPU, it has 2 interface Ethernet port X2 P1R and X2 P2R. Thank you very much for your replying, Best regards, Steven AttachmentDesktop.zip (135 Downloads) |
1/18/2012 12:34 PM | |
Posts: 19 Rating: (0) |
Dear, I already ordered one MMC from Siemens Distributor, for temperaty using I can use any MCC (SD card) not siemens? Thank you, Best regards Steven |
1/19/2012 1:06 AM | |
Posts: 19 Rating: (0) |
Dear Wizard, Thank you for your replying. Best regards, Steven |
7/20/2012 12:07 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, If this MMC size is enough for the project it should be not a probelm for CPU. Best regards, Hristo Mihalev
|
Follow us on