7/23/2012 1:45 PM | |
Posts: 14 Rating: (0) |
Hello guys! I figured out the SCL example from the module C-series (square of a number), and now I would like to figure out similar,but far more complex example from the SCL manual - chapter 3 - measured value acquisition ( http://support.automation.siemens.com/WW/view/en/5581793). The source code itself is written in the manual, but I have some problems joining it all, symbol table etc. So I was wondering if there exists the whole project file somewhere to download, I cant find it? Thanks |
Last edited by: O_Moderator at: 7/23/2012 2:53 PMlink edited Last edited by: vasso123 at: 7/23/2012 1:45 PM |
|
7/23/2012 2:47 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hello, See this sample project in STEP7 "ZEN05_01_S7SCL__Measv06" Best regards, Hamid Hosseini |
Last edited by: O_Moderator at: 7/23/2012 2:53 PMlink edited |
|
This contribution was helpful to1 thankful Users |
7/24/2012 8:02 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello, What do you think about reading section 4.10.1 of the mentioned document? S7-SCL V5.3 for S7-300/400
Best regards, Hamid Hosseini |
Follow us on