Industry Online Support
Technical Forum
7/11/2012 10:55 PM | |
Posts: 1 Rating: (0) |
Hello, Program is running on 64-bit WINDOWS 7. Everything is fine, except for help. When I start Starter appears to me, the screen as in Picture 1 in attachment. I found on this forum (/tf/WW/en/Posts/23383 on last post) next advise: "OR 3. Select any of the chm-files; right mouse-click, properties. Click onto "Zulassen" (means allow) and this file will be shown. see attachment" Now help tipps is only partially open, some stuff is okay, but not for others. Does anyone have similar problem and what is sollution for it? Thanks in advance
Attachmentpicture 1.pdf (613 Downloads) |
7/12/2012 9:25 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, I guess you check suggestion 1 too. Anyway try it with reinstall now. If not works again -Support Request Best regards, Hristo Mihalev
|
8/3/2012 1:38 PM | |
Posts: 2 Rating: (0) |
Copy the installprogram to a USB stick and install then from the USB stick the program. |
Follow us on