Industry Online Support
Technical Forum
8/21/2012 12:11 PM | |
Posts: 2 Rating: (0) |
hello friends i am a beginner to logo programming who needs your help one of my senior taught me reverse forward dol starter. in this program we have used e.stop and motor off push button. from these we gave input to "and" gate block boo1. the inputs are not inverted. another program for simple dol starter i downloaded from one of the threads. in that program the programmer used inverted input to "and" gate from motor off button. please explan. AttachmentREV FWD DOL.zip (203 Downloads) |
8/21/2012 12:13 PM | |
Posts: 2 Rating: (0) |
here is the other program
AttachmentDOL Starter fbd.zip (208 Downloads) |
8/21/2012 1:47 PM | |
Posts: 378 Rating: (73) |
Dear somnolent , Well Come to the forum! If you are beginner for LOGO and familiar to other PLC program, I suggest you to start with ladder diagram instead of FBD. You can convert FBD diagram to LAD or viceversa by clicking Covert to LAD at the top right of LOGO Soft tool bar ( I have attached here the ladder diagram of your program). Then you can simulate and observe the function. The two programs are different. Your program DOL Starter fbd is a simple start/stop program with output latch but there is redundant AND block, you can make it further short. Your program REV FWD DOL program is forward reverse motor control. The two programs are totaly different that is why the usage of block B001 is different. Once again convert to LAD to make it easily understandable. Regards AttachmentLadder diagram.zip (213 Downloads) |
This contribution was helpful to1 thankful Users |
8/30/2012 12:44 PM | |
Posts: 378 Rating: (73) |
Hi Zazu, You have said more than two pence worth !!! I hope every thread's example programs will not be downloaded directly to the machine without keeping saftey and circuit standards. Good Day! |
Follow us on