Industry Online Support
Technical Forum
9/3/2012 2:11 AM | |
Joined: 1/10/2012 Last visit: 9/10/2024 Posts: 24 Rating: (1) |
Hi there, During Runtime, check the connection status. In WinCC Explorer, go to tools menu -> status of Driver connections. If status is disconnected, try checking the following: 1) In system parameter, check logical device name (see attached file), this should pint to your CP 5611 card. 2) In connection properties (see attached file), check the connection parameters. Frequently Station address (your PLC MPI address) or slot number are not correct. Note that for S7-300, slot number is 2. 3) check your CP-6511 address. This should differ from PLC's address. AttachmentMy Pictures.zip (112 Downloads) |
Best Regards, |
|
Follow us on