Industry Online Support
Technical Forum
8/7/2012 10:52 AM | |
Posts: 163 Rating: (4) |
Respected Sir, I have S7 300 memory card of 128 KB which contain a password protected program. So inorder to delete it, I inserted it in field PG and from File--> S7 memory card, selected 'Delete' option. But ther is an error in the process showing that "EPROM : the MMC is defective".And in its Help file it is written that " MMC is formated by other hardware". Please help me how to reset it or is it really defective?.... (pl check the attachment--->printscreen of error) Regards, Rudrani
Attachmenterror.zip (188 Downloads) |
8/7/2012 10:57 AM | |
Posts: 1064 Rating: (72) |
You need to replace the memory card Sorry |
8/7/2012 10:59 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, If you have another CPU you can try How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? Bur i'm afraid it's to late for this MMC, someone tried to erase it with windows? Regards, Marcjan |
Last edited by: Marcjan at: 8/7/2012 11:01 AMProblem solved? |
|
9/15/2012 12:21 AM | |
Posts: 3 Rating: (0) |
not really... |
Follow us on