9/18/2012 12:19 PM | |
Posts: 4 Rating: (0) |
V5.5 and does not see the adapter. |
Last edited by: Walter28 at: 9/18/2012 12:20 PM |
|
9/25/2012 9:47 AM | |
Posts: 376 Rating: (57)
|
Hello Walter28, in the STEP 7 function set PG/PC interface you can stillcheck the following. If the required interface PC Adapter USBis not available, click on the "Select" button and install the relevant driver in the "Install/Remove Interfaces" dialog. In this case mark the required interface in the "Selection:" window on the left and click on the "Install -->" button. After installation the interface is shown in the "Installed:" window on the right. Then close the dialog and select the interface in the "Interface Parameter Assignment Used:" dialog. Close the PG/PC interface with OK. |
Follow us on