10/19/2012 2:23 PM | |
Posts: 4 Rating: (0) |
Hello all, Long time reader first time poster!! Have a simple application using a CPU224 with a TD200 connected. I set up the TD through the wizard - it only needs to display 2 parameters Good Count/Bad Count and then use F1 to reset counts. The problem i'm having is i get the error no parameter block on the TD - if i press ESC and go to view messages i can see my messages and my counts. After a while it will revert to No parameter block. The values in my counts also don't update live, as in if i press ESC and go back into the message my values are updated - I've looked through the forum and changed my program in various ways as described in posts I've read but to no avail. If someone could help me out. that would be great. I've attached a copy of the program for you to look at. The CPU is REL 01.21 and the TD is REL 2.01 Many thanks in advance....
AttachmentPart Checker.zip (40 Downloads) |
10/19/2012 3:16 PM | |
Posts: 4 Rating: (0) |
Hi Marcjan, Communications are all ok, my block address is 0 - yet i still get the error?
|
10/22/2012 8:41 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, I created a new TD with same data and now it's working All i changed is the F-key byte(byte 4 to 30, it was writing in Good count MD4. See attached program, Please change CPU back to your CPU Regards, Marcjan AttachmentPartCheckMC_1.zip (59 Downloads) |
Problem solved? |
|
Follow us on