Industry Online Support
Technical Forum
10/16/2012 6:48 PM | |
Joined: 6/11/2012 Last visit: 12/3/2023 Posts: 38 Rating: (0) |
Hi all. I have problem with my analog input card 6ES7 331-7KF02-0AB0. CPU is 315-2PN/DP. With analog card i need to measure temperature via pt100. When i set in HW configuration analog input card measuring type resistor RT and measuring range pt100std., and download to PLC, red led on AI card indicate SF. When i set back to default measuring type (voltage E) and download to PLC, red led turn off. In case when i choose RT, inputs shows number 32767 in VAT table as DEC type, in E case inputs shows 0 as DEC type. In attachemt you have wiring example of PT100 and HW analgog input card settings. Please help me to resolve this problem. Tnx. AttachmentAttachemt.zip (102 Downloads) |
10/16/2012 7:36 PM | |
Joined: 6/11/2012 Last visit: 12/3/2023 Posts: 38 Rating: (0) |
I will check it tomorrow. Tnx a lot |
Follow us on