Industry Online Support
Technical Forum
10/30/2012 12:55 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello, we have a server project with several clients. I'm working on some things where I want runtime with alarm logging, so I deleted the server data. I added some pictures, scripts, nothing special. But I've had several times, randomally that when opening a picture in the graphics designer, whole WinCC freezes... Doesn't matter which picture. The project is opened on Win XP3, WinCC 7.0 SP3 on a VM station. I already tried opening the project in my PCS7 8.0, but also the project freezes when opening a picture. Everything else works...the diagnose files show no problems during the time WinCC freezes.. Can somebody help me with this? As I don't know where to start from... The project is upgraded to v7.0 |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on