Industry Online Support
Technical Forum
11/9/2012 4:08 PM | |
Joined: 8/11/2006 Last visit: 3/25/2024 Posts: 29 Rating: (0) |
Hi men, is not the first time than when I try to use WinCC Flexible appear a message-box with a message "A serious error occured (0x8013141a). Please contact ..." (can see the full message attached). To solve this problem, the only way that I find, is remove and reinstal completely WinCCFlex. But now happen again! And not only on my notebook, on my collegue, too!! From the first time, is passed a few days (less than one month. No other software was istallaed (only windows update, and antivirus - AVAST, maybe!). Any suggestions would be appreciated. I'm using VMWare 8.0, with windows XP SP3 OS AttachmentErrorMessage.zip (96 Downloads) |
11/9/2012 4:41 PM | |
Posts: 3037 Rating: (192)
|
Hello GP68, Do you use a HP Notebook? Then is this the solution. What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook? /tf/WW/de/Posts/79706 Tweety |
11/12/2012 3:36 PM | |
Posts: 3037 Rating: (192)
|
Hello GP68, You should start a support request. support request Tweety |
Follow us on