Industry Online Support
Technical Forum
11/26/2012 8:28 AM | |
Posts: 10 Rating: (0) |
Hello Experts, Attached is the connection diagram of the danfoss drive i am migrating to 440. My connections as follows: Terminals 5 and 9 for the starting, terminal 19 and 20 for the feedback running signal, then terminal 3 and 4 for the speed reference from the PLC. Also i have the config as follows: P700=2,P1000=2,P756=3,P759=18,P760=80%,P757=4mA,P2000=50Hz. The problem iam having is that the PLC does not control the speed of the drive, but on r752=19.9 permanently. Kindly assist on this issue, P1080=0,P1081=50hz. The drive runs to 40hz when it is started and does not take any reference from the allen bradely PLC. Kindly assist. AttachmentC:\Users\yef04751\Desktop\DriveConnection.pdf (121 Downloads) |
Follow us on