6/24/2011 4:49 PM | |
Posts: 8 Rating: (0) |
Hello Expert Forum Members, I have a 314 system configured: 1. PS307 2. 314 MPI CPU 4. SM321 5. SM322 6. SM338 7. FM350 8. FM350 9. SM331 They system has been working without any problems for the last 6mths. It has just start to intermittently go into STOP mode. The system is physically remote to me hence error info is a bit sketchy. On one occasion all SF leds were solid red with the exception of the sm331 which was flashing. On otheroccasions only the CPU had theSF led on. Attached is a CPU diag file from the system - but not necessarily related to the above SF LED indications (I was unable at the time to download the diagnostics log). I would be grateful if anyone knows, from this limited info, what the fault is likely to be or do I need to load the diagnostic OB's to get to get the exact cause of the problem? Thanks Fozz AttachmentDiagnose2.zip (205 Downloads) |
6/24/2011 7:44 PM | |
Posts: 947 Rating: (45) |
Hi Fozz Operating mode: STOP (own initialization)
|
Follow us on