Industry Online Support
Technical Forum
12/29/2012 5:16 PM | |
Posts: 1 Rating: (0) |
I had a go at above but failed miserably. Here is what I am trying to achieve and this is found in the Autocycling network of FC01 attached: 1) When main pump is on (M100.1) and autocycling inputistriggered (M100.4) and actuator is homed (I1.7), Autocycling switches on ( M100.5). This works 2) When autocycling (M100.5) is on, solenoid A(M100.6) is switched on for 5 seconds. After 5 seconds, it is switched off and solenoid B ( M 100.7) is switched on for 5 seconds. This cycle repeats for 100 cycles after which the autocycling output ( M 100.5) is reset. When it is triggered again using ( M 100.4), the cycling repeats. This I believe is fundamental logic but I am new to it, so had a go but did not succeed. Any comments/support will help Kind Regards KWaris AttachmentStl.zip (72 Downloads) |
Follow us on