Industry Online Support
Technical Forum
1/27/2013 3:47 PM | |
Joined: 7/17/2010 Last visit: 2/17/2024 Posts: 184 Rating: (0) |
Hi people. I go develop one totalize of flow water, but my idea of software it's Flow variable the 0 at 25 T/h Então 0 - 25 t/h convert 0-6,944 kg/s Calculate: (((Flow/3600)*1000)/32000) = Kg Exemplo (((25/3600)*1000/3200)=0,000217014 kg know accumulator 1 = MD100+0.000217014=MD100 when accumulator accumulator >= 4608 accumulator 2 = MD200+1=MD200 and Sub 0.00217014 of accumulator 1 But using time of the second of accumulator flow.. The ideai is good. Attachmenthome.zip (117 Downloads) |
1/28/2013 5:26 AM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (221) |
Hello Martins_Eng, A sample projectis available here as a FAQ - How can you add together physical flow measurements (mass flow rate, for example) to a total value in STEP 7 (TIA Portal) V11? |
Like it? Rate it! |
|
1/28/2013 10:55 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Totalize in S7-1200 Best regards O_Moderator |
Follow us on