Industry Online Support
Technical Forum
1/31/2013 5:30 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello hamza; From the CEMAT manual: Engineering Manual V7.1 1. Plant Hierarchy The picture hierarchy and the summarizing indications are derived from the plant hierarchy. For this reason the charts as well as the pictures must be assigned to the correct hierarchy folders, even if the block icons are not created automatically 2. Creating the plant hierarchy:: You can use the Wizard to create a new Project or Multiproject or you can create the Project or Multiproject manually. The wizard will create a Project Structure with Plant Hierarchy which you can modify or delete. In the following description the project is created manually: In the SIMATIC Manager create a new project using File -> New. Select Type Multiproject and define the Project name. Check the Storage location (it should be the Multiproject directory). Select the Multiproject in the SIMATIC Manager and use Multiproject -> Create in Multiproject to create the first Project within the Multiproject. 3. Hierarchy folders: For a Cement plant 3 hierarchy folders should be (more than) enough. For the diagnostic of the hardware up to 8 hierarchy levels are required. If you want to derive the diagnostic screens from the plant hierarchy, you have to select the function "Derive diagnostic screens from the plant hierarchy". With the OS Area you specify which Hierarchy level is used the Selection Buttons in the Overview Area. Also the Operator right can later on be specified per Area. The picture hierarchy must be derived from the plant hierarchy. Otherwise some functions cannot be guaranteed any more. During OS Compile the WinCC Picture tree is then generated automatically. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/31/2013 5:32 PM |
|
This contribution was helpful to1 thankful Users |
2/1/2013 10:55 AM | |
Posts: 45 Rating: (0) |
Thanks brother daniel, i will try to uninstall it and install again the PCS7,it's pleasure to talk to you my Friend. |
Follow us on