2/1/2013 3:09 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Dear Mr. / Ms.Piscean 2010, First of all, all the datasfor the SIEMENS synchronous servo motors are found in the configuration manual, e.g. for the 1FK7 Generation 2 http://support.automation.siemens.com/WW/view/en/55379345 There are the rated speed and the no of ple pairs given. The base frequency is calculated by f=n*p/60 (speed * no pole pairs /60) By using theSINAMICS S system, the necessary data are included and loaded during the commissioning by choosing the motor via the order no. |
With best regards, |
|
Follow us on