Industry Online Support
Technical Forum
2/8/2013 2:48 PM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (9) |
Can ET200SP be used on Simotion? I cannot find it in the hardware catalog |
2/8/2013 3:22 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, have you installed the GSD Files for ET200SP ? Regards Christoph |
2/8/2013 3:28 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello David; I agree with Christoph: SIMATIC ET 200SP ET 200SP distributed I/O system ConfigurationThe ET 200SP is mounted on a mounting rail and consists of: · An interface module that communicates with all IO controllers that behave in accordance with the PROFINET standard IEC 61158 · Up to 32 I/O modules that are connected to passive BaseUnits in any combination · A server module that completes the configuration of the ET 200SP You will be able to download the GSDML file for the ET 200SP from this link: PROFINET GSD files : ET 200SP Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/8/2013 3:34 PM |
|
Follow us on