2/19/2013 4:01 AM | |
Posts: 7 Rating: (0) |
Hello TechTeam! I don't have any warnings/alarms in the drive or in the CLP. I'm not using any specific communication protocol. I am sending the software of Starter in attachment.The software of TIA Portal, the file is too large to attach in the topic.
Thanks for the help. AttachmentBarkhausen.zip (112 Downloads) |
Last edited by: O_Moderator at: 2/19/2013 7:53 AMlink deleted |
|
2/20/2013 3:38 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, I have checked your project. Its an unusal way to combine the control unit communication with BICO connections to the drive - but its possible that this can work. You should implement an additional control bit to acknowledge faults on the drives. Normaly it should be possible to run the drives. I have attached an example project for TIA Portal with S7-1200 and Sinamics S110. Maybe this can give you a help for starting the communication. This example is using the blocks DP_RD_DAT and DP_WR_DAT. AttachmentD:\temp\S7_1200_CU305PN_TIA11SP2.zip (121 Downloads) |
With best regards, |
|
Follow us on