Industry Online Support
Technical Forum
2/25/2013 1:09 PM | |
Posts: 206 Rating: (22) |
Hi JGregorio, the discription of FB41 you find in the manual of the Siwarex FTA http://support.automation.siemens.com/WW/view/en/17970155chapter 8. In the actual GettingStarted project http://support.automation.siemens.com/WW/view/en/25296061there is no. FB31 in thid project. I don't know what for it is and how it works. Regards ABenno |
2/26/2013 9:54 AM | |
Posts: 206 Rating: (22) |
Hello JGregorio, please excuse, I didn't get it at the beginning, you are talking about the Multifill package. This project was made for small batch applications. The FB31 is the block that handles the communication between the batch processand the Siwarex FTA FB41. In the manual of the Multifill package page 5-19 you find the internal function of theFB31. The manual you find here: http://support.automation.siemens.com/WW/view/en/18713925 Normally it is not necessary to knowhow the FB's work in internally. Roughly the function of the project is as follow: - If the batch is started, - the TaskManager (TM, FC40)is looking for a recipie line (in DB31,Db_Task_Act_List)that is not finished, - the TM is lookingif the device (mostly a scale) for this line is free, - if the device is free the TM will load the Set point and the material parameters - with these parameters the TM will start the device - if the device has finished the TM will finish the recipe line. - if all line are finished the TM will finish the batch process. Regards ABenno |
Follow us on